What does 'continue_dll_off_1' mean?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

What does 'continue_dll_off_1' mean?

跳至解决方案
1,888 次查看
JHY
Contributor IV

linux version : 3.0.35

./ltib/rpm/BUILD/linux/arch/arm/mach-mx6/mx6_ddr_freq.S (line 485)

    /* if DLL is currently on, turn it off
    cmp     r9, #1
    beq     continue_dll_off_1

There is an commented block but comment is not closed, is it right?

The commented code does not make trouble but looks untrustworthy,

Best regards.

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
1,767 次查看
igorpadykov
NXP Employee
NXP Employee

Hi JHY

this (unfinished comment) was fixed in latest L3.0.101_4.1.1 release:

ENGR00320182 [iMX6DQ/iMX6DL] Fix bug in DLL off mode code in DDR3 frequency change procedure

L3.0.101_4.1.1_SOURCE_BSP : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite Linux BSP Source Code Files.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,768 次查看
igorpadykov
NXP Employee
NXP Employee

Hi JHY

this (unfinished comment) was fixed in latest L3.0.101_4.1.1 release:

ENGR00320182 [iMX6DQ/iMX6DL] Fix bug in DLL off mode code in DDR3 frequency change procedure

L3.0.101_4.1.1_SOURCE_BSP : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite Linux BSP Source Code Files.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复