I use i.MX28, uboot and spl.
After board_init_ll (SPL) returned, before board_init_f (uboot) executed, 'Undefined Ins' is printed out in my console and system is hanging.
I can not find 'Undefined Ins' in uboot or spl source.
What is it executed between SPL and uboot.
解決済! 解決策の投稿を見る。
It is likely that the "Undefined Instruction" been printed by ROM code. And ROM code should print "r14_undef" and followed with LR value which points the place where the exception occurred. Do you see these ever?
B.R
Jerry 
Also, I've seen cases where 'Undefined Ins' was caused when the wrong toolchain was used: for example - using a toolchain for armv7 (mx6) to build code for arm926 (mx28). Make sure you have a suitable toolchain for mx28.
It is likely that the "Undefined Instruction" been printed by ROM code. And ROM code should print "r14_undef" and followed with LR value which points the place where the exception occurred. Do you see these ever?
B.R
Jerry 
Please make sure you follow the procedures below:
http://git.denx.de/?p=u-boot.git;a=blob;f=doc/README.mxs;h=ed2e5688562ac1af55a7c6213f5f3eb825e055b8;...
and
http://git.denx.de/?p=u-boot.git;a=blob;f=board/freescale/mx28evk/README;h=958ebc679106a52810506c506...
Please take a look at this past thread, it might be able to help you: