What are all the Linux-kernel versions compatible with the Android 11.0.0_2.2.0 using i.MX8MQ EVK?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What are all the Linux-kernel versions compatible with the Android 11.0.0_2.2.0 using i.MX8MQ EVK?

925件の閲覧回数
Iyshwarya
Contributor I

What are all the Linux-kernel versions which are compatible (so that I should not get any checkvinff error) with the Android 11.0.0_2.2.0 using i.MX8MQ EVK? And replacing the separately built kernel Image alone of the supported version to the Android source code helps me to upgrade the kernel?

0 件の賞賛
返信
1 返信

907件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

refer to the release note, android 11.0.0_2.2.0 uses Linux 5.10.35 kernel

0 件の賞賛
返信