Hello community,
after I make some experience with different images of Linux I want to do the next step.
I think there a a lot of ways of programming a application.
I just want a simple graphic user interface, gpio and other hardware programming and not to much overhead.
My preferred language is C. My Hardware is a Sabrelite.
I have made experience with Cortex M3/M4 programming, so it is not easy to get the right way on this new land :smileyhappy:
Be free and outer what you think.
regards 
Joerg
Solved! Go to Solution.
1. Download latest BSP (for to the main MX6 page on freescale.com)
2. Follow the User Guide. Basically you install LTIB and do a build
3. Follow the QT page you sent me.
4. Flash the resulting image into a SD.
Leo
Hi Joerg,
I am not a programmer but I believe for scalability, you should use QT. Search on the community about ways to install QT4/5. In case you want an image with QT installed, try Yocto,
Leo
 
					
				
		
Hello Leo,
I have tried Yocto on the Board. It is nice, but I didn't find a working How To to set up the Host PC.
This one Building QT for i.MX6 looks good and it worked for me till I should set the Path:
$ export PATH=$PATH:/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/
I don´t find where to download that.
regards
Joerg
Do a LTIB build (try the minimal profile) with latest BSP (400). I have it on my PATH
b42214@vfae-server:~/fsl/BSP/src/linux/L3.0.35_4.0.0_130424/ltib$ ./ltib -m shell
Entering ltib shell mode, type 'exit' to quit
LTIB> echo $PATH
/home/b42214/fsl/BSP/src/linux/L3.0.35_4.0.0_130424/ltib/bin:/opt/freescale/ltib/usr/spoof:/home/b42214/fsl/BSP/src/linux/L3.0.35_4.0.0_130424/ltib/bin:/opt/freescale/ltib/usr/bin:/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin:/usr/local/bin:/usr/bin:/bin:/usr/bin/X11:/usr/X11R6/bin
LTIB>
 
					
				
		
I'm not sure to do that. I read now for a while on the ltip.org side. There is a lot of things I have to understand and to do before I could do that. Or there is a How To for i.mx6 that I don't find on search the freescale forum?
regards
Joerg
1. Download latest BSP (for to the main MX6 page on freescale.com)
2. Follow the User Guide. Basically you install LTIB and do a build
3. Follow the QT page you sent me.
4. Flash the resulting image into a SD.
Leo
 
					
				
		
Hello Leo,
I still struggle on building Ltip.
For the first errors I find a solution on google but for this I don't find anything.
Processing platform: Host support packages
============================================
using /home/joerg/ltib/config/platform/host/ltib.preconfig
Processing: fake-provides
===========================
Processing: mkspooflinks
==========================
Processing: distcc
====================
Processing: ccache
====================
Processing: bison
===================
Processing: flex
==================
Processing: texinfo
=====================
Processing: autoconf
======================
Processing: libtool
=====================
Processing: lkc
=================
Processing: patch
===================
Processing: wget-ssl
======================
can't find spec file for wget-ssl
traceback:
main::build_rpm:783
main::f_buildrpms:1077
main::build_host_rpms:1492
main::host_checks:1554
main:562
Started: Tue Jun 25 07:07:52 2013
Ended: Tue Jun 25 07:07:52 2013
Elapsed: 0 seconds
VERSION : 13.2.1
CVS_VERSION : $Revision: 1.91 $ (Savannah)
PLATFORM : host
GNUTARCH : x86_64
TOOLCHAIN :
TOOLCHAIN_CFLAGS :
Build Failed
Joerg 
Which profile are you trying to compile? try the minimal profile first (to select this, just type ./ltib -m selectype) or deselect the failed pkg (./ltib -m config). In both cases, run ./ltib again.
Leo
 
					
				
		
joerg@joergwenglish:~/ltib$ ./ltib -m selectype
Installing host support packages.
This only needs to be done once per host, but may take up to
an hour to complete ...
If an error occurs, a log file with the full output may be found in:
/home/joerg/ltib/host_config.log
If you would like to see the log messages as the host packages are built and
installed:
   * Open another terminal in the same directory
   * Run the command: tail -f host_config.log
   * When you're done with the tail, use CTRL+C to exit
Exiting on error or interrupt
Please see >> /home/joerg/ltib/host_config.log for details
Both ends with the same result. can find spec file wget-ssl
Joerg
have you installed all needed HOST packages for ltib?
Leo
 
					
				
		
My mistake, I used the ltip from ltip.org
I have to use that one from BSP Package.
Thank You Leo for help
Joerg
 
					
				
		
/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/../lib/gcc/arm-fsl-linux-gnueabi/4.6.2/../../../../arm-fsl-linux-gnueabi/bin/ld: cannot find /lib/libc.so.6
/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/../lib/gcc/arm-fsl-linux-gnueabi/4.6.2/../../../../arm-fsl-linux-gnueabi/bin/ld: cannot find /usr/lib/libc_nonshared.a
/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/../lib/gcc/arm-fsl-linux-gnueabi/4.6.2/../../../../arm-fsl-linux-gnueabi/bin/ld: cannot find /lib/ld-linux.so.3
collect2: ld returned 1 exit status
make: *** [busybox_unstripped] Error 1
error: Bad exit status from /home/joerg/ltib/tmp/rpm-tmp.12076 (%build)
RPM build errors:
Bad exit status from /home/joerg/ltib/tmp/rpm-tmp.12076 (%build)
Build time for busybox: 5 seconds
Failed building busybox
f_buildrpms() returned an error, exiting
traceback:
main:572
Started: Wed Jun 26 14:31:14 2013
Ended: Wed Jun 26 14:31:19 2013
Elapsed: 5 seconds
These packages failed to build:
busybox
Build Failed
Exiting on error or interrupt
joerg@joergwenglish:~/ltib$
Now I think I have done everything right but it fails again...
What Linux OS are you using?
ltib.org, not ltip.org :smileyhappy:
Leo
 
					
				
		
Ubuntu 12.04.2
Hi,
Not sure how to solve your issue. One thing you can try, is to download prebuild images, then mount the rootfs.ext2 on your host, and use that rootfs when compiling QT. This way you do not need to deal with compilation issues.
Leo
 
					
				
		
that helps, see last reply