Weston problem on parallel lcd display

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Weston problem on parallel lcd display

ソリューションへジャンプ
3,859件の閲覧回数
davideballestre
Contributor I

Hi,
we are running BSP 5.15.71_2.2.0 on a custom board with a parallel lcd display and imx6dl microprocessor. We are facing a problem with weston surface g2d-renderer. only vertical stripes are visible (see attached image).
It seems a pixel format problem but framebuffer is working well and weston logs are ok.
Without "use-g2d=1" weston fails to start with "failed to create egl surface" (see attached log).
Can you help me?

Thanks

Davide

ラベル(1)
0 件の賞賛
返信
1 解決策
3,822件の閲覧回数
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @davideballestre,

I hope you are doing well
 
My apology for the delayed response.
Please try to set the bpp value for the Weston to <16> from the device tree.
 
Thanks & Regards,
Dhruvit Vasavada

元の投稿で解決策を見る

2 返答(返信)
3,823件の閲覧回数
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @davideballestre,

I hope you are doing well
 
My apology for the delayed response.
Please try to set the bpp value for the Weston to <16> from the device tree.
 
Thanks & Regards,
Dhruvit Vasavada
3,803件の閲覧回数
davideballestre
Contributor I

hi!
everything well here! with your solution weston works great now (see attached image).

thank you very much for your help.

regards
davide

 

 

0 件の賞賛
返信