Wayland Protocol error : Popups created with parent which is not topmost with xdg-shell-v6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Wayland Protocol error : Popups created with parent which is not topmost with xdg-shell-v6

2,494 次查看
deeksha
Contributor III

Hi All,

I'm using 4.14.98 Sumo i.MX8M Mini board with qt 5.10.1,  X-Wayland Server.

When I'm trying to run qt application with combo-box, submenu. Application is terminating with

following errors when I click on it.

Using Wayland-EGL Using the 'xdg-shell-v6' shell integration zxdg_shell_v6@17: error 2: xdg_popup was not created on the topmost popup The Wayland connection experienced a fatal error (Protocol error).

How this error can be solved. Please do the needful.

Thanks in advance,

Regards,

Deeksha

0 项奖励
回复
2 回复数

2,477 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

I tested xdg-shell-v6 on L5.10.XX and there is no issue when run qt demo.You can try newest BSP

0 项奖励
回复

2,472 次查看
deeksha
Contributor III

Hi

Thanks for your reply.

As I'm working L4.14.98 , cannot update BSP due to internal reason.

So could you please help me in resolve this issue.

Regards,

Deeksha

0 项奖励
回复