Way of system reset by software

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Way of system reset by software

981 次查看
toshiharu_shimi
Contributor II

I would like to assert system reset by software.

I intend to use Software Reset Signal(SRS) in Watch dog Control Register, But errata report mentions that watchdog timeout or software trigger will not reset the SOC.

Is there other way to assert system reset by software?

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

942 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Toshiharu

>Is there other way to assert system reset by software?

not, sorry. So recommendation is to remove power (Voltage source) to
all components on the board in the event of a processor reset.

NXP reference boards were designed to remove power (Voltage source)
to all components on the board in the event of a processor reset.

For example on i.MX7D Sabre SD schematic SPF-28590 p.23 

it is done with signal PMIC_PWRON, U37.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复