Watchdog rebooting kernel

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Watchdog rebooting kernel

ソリューションへジャンプ
3,757件の閲覧回数
chandraevolute
Contributor V

I am working with watchdog now

I wrote a small piece of code to understand the working of software watchdog

#include <stdio.h>

#include <stdlib.h>

#include <string.h>

#include <unistd.h>

#include <fcntl.h>

#include <sys/ioctl.h>

#include <linux/types.h>

#include <linux/watchdog.h>

void Keep_Alive(int fd)

{

//      int options = 0;

        int pretimeout = 10;

        int options = 0;

        ioctl(fd, WDIOS_ENABLECARD, &options);

        ioctl(fd, WDIOC_SETPRETIMEOUT, &pretimeout);

//      ioctl(fd, WDIOC_SETOPTIONS, &options);

        printf("Watchdog Alive \n");

}

void Kill(int fd)

{

        write(fd, "V", 1);

        printf("Watchdog killed\n");

}

int main()

{

        int fd;

        int timeout = 15;

        fd = open("/dev/watchdog", O_WRONLY);

        if(fd == -1)

        {

                fprintf(stderr, "Watchdog faild to open");

                return ;

        }

        else

        {

  ioctl(fd, WDIOC_SETTIMEOUT, &timeout);

                printf("The timeout was set to %d seconds\n", timeout);

        }

        while(1)

        {

                Keep_Alive(fd);

                sleep(10);

        }

//      Kill(fd);

}

Output :

root@imx6ulevk:/media# ./WatchDog

The timeout was set to 15 seconds

Watchdog Alive

watchdog pre-timeout:10, 5 Seconds remained

Watchdog Alive

U-Boot 2015.04-imx_v2015.04_3.14.38_6ul_ga+g5d63276 (May 16 2016 - 14:32:19)

I am kicking the watchdog for every 10 seconds still the board is rebooting after 15 secs.

What is the wrong i am doing.

i am using imx6ulevk board and 3.14.38 kernel.

ラベル(3)
タグ(2)
0 件の賞賛
返信
1 解決策
3,068件の閲覧回数
chandraevolute
Contributor V

my bad i overlooked the options of watchdog.

I changed   ioctl(fd, WDIOC_SETPRETIMEOUT, &pretimeout); this line to  ioctl(fd, WDIOC_KEEPALIVE, &options);

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,068件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi chandra

one can check if serviced correctly WDOGx_WSR register :

0x5555 Write to the Watchdog Service Register (WDOG_WSR).

0xAAAA Write to the Watchdog Service Register (WDOG_WSR).

use, for example memtool and try to reset wdog.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,068件の閲覧回数
chandraevolute
Contributor V

Hi igorpadykov

How can I write values directly to resgisters in linux?? How can I check the register values?

0 件の賞賛
返信
3,069件の閲覧回数
chandraevolute
Contributor V

my bad i overlooked the options of watchdog.

I changed   ioctl(fd, WDIOC_SETPRETIMEOUT, &pretimeout); this line to  ioctl(fd, WDIOC_KEEPALIVE, &options);

0 件の賞賛
返信