Watchdog reboot on overloading IPU with Linux 4.1.15 in iMX6Q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Watchdog reboot on overloading IPU with Linux 4.1.15 in iMX6Q

2,862 Views
ivyliu
Contributor IV

Hi,

We are using Linux 4.1.15 in iMX6Q (iMX6Q). The display resolution is 1920x120

When we overloading IPU by keep queuing a buffer to IPU for displaying in a gapless loop, and with watchdog enabled, the monitor will reset randomly, in 30min - 11 hours. This issue happened in room temperature. 

When the watchdog is disabled, there is no issue with the same test.

The issue happened very randomly, we have thought about the CPU temperature, but when we increased the CPU temperature to 60C - 80C, the issue did not happen.

Have someone had the similar issue?

Could someone help us with this issue?

Thanks and Best Regards,

Ivy

Labels (3)
0 Kudos
Reply
7 Replies

2,802 Views
ivyliu
Contributor IV

@joanxie  Hi Joanxie,

 Do you have any thoughts on this issue?

Thanks and Best regards,

Ivy

0 Kudos
Reply

2,855 Views
joanxie
NXP TechSupport
NXP TechSupport

did you test your own customized board, right? all of boards have this issue or only some of them?

0 Kudos
Reply

2,845 Views
ivyliu
Contributor IV

Hi Joanxie,

Yes, it is on our customized board. The issue happens on >95% boards.

Thanks and Best Regards,

Ivy

0 Kudos
Reply

2,844 Views
ivyliu
Contributor IV

Hi Joanxie,

Yes, it is on our customized board. It happened on >95% boards.

Thanks and Best Regards,

Ivy

0 Kudos
Reply

2,745 Views
joanxie
NXP TechSupport
NXP TechSupport

I have already  mailed to you, pls check

0 Kudos
Reply

2,735 Views
ivyliu
Contributor IV

Hi Joan,

Not sure why I did not get your email.

Could you please help to send it again?

 

Thanks and Best Regards,

Ivy

0 Kudos
Reply

2,710 Views
joanxie
NXP TechSupport
NXP TechSupport

did you get support from any distributor? I got the same questions from them, if yes, pls contact them

0 Kudos
Reply