Watchdog on imx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Watchdog on imx

2,989件の閲覧回数
matt67
Contributor III

Hello,

What do you think of using the imx internal watchdog timer with fsl,ext-reset-output dts property to output reset signal to PMIC ?

Is it safe enough, and guaranteed that the Low frequency reference clock feeding the WDOG block doesn't stop in case of hanging ?

Or perhaps should I use an hardware reset handler ?

ラベル(3)
タグ(2)
0 件の賞賛
返信
3 返答(返信)

2,688件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi matt67

yes using internal watchdog to reset pmic is fine solution and it is safe.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,688件の閲覧回数
matt67
Contributor III

HI Igor,

It is safe also in u-boot ? Is it possible in u-boot to use the GPIO outpout from the watchdog ?

0 件の賞賛
返信

2,688件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi matt67

 

yes it is safe also in u-boot.

 

Best regards
igor

0 件の賞賛
返信