Watchdog imx6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Watchdog imx6

1,782件の閲覧回数
ifzhao
Contributor I

hi, all

Imx6 duallite with BSP 4.3 is used here. Android system is running. But sometime it reboot, and the boot type is watch dog.I 've kept record both of logcat and kmsg. But find nothing, it's so strange.!!

this is setting of watchdog:

<3>[ 14.988727] init: watchdogd:getsupport indent=0x8380
<3>[ 14.993958] init: watchdogd:getstatus flags=0x0
<3>[ 14.998648] init: watchdogd:getbootstatus flags=0x0
<3>[ 15.003757] init: watchdogd:gettimeout = 30
<3>[ 15.008113] init: watchdogd:getpretimeout = 5

if the reboot is caused by watchdog, why there is no exception or kernel crash or any other abnormal printing in kernel and logcat ? If not, what's this shit?

ラベル(2)
0 件の賞賛
返信
1 返信

1,423件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 The watchdog usually provides SOC hardware reset, this does not allow using system interrupts.
Moreover, NXP recommends do not use just SOC reset, but - to implement total system POR instead,

via external circuit.

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 件の賞賛
返信