Watchdog imx6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Watchdog imx6

879 Views
ifzhao
Contributor I

hi, all

Imx6 duallite with BSP 4.3 is used here. Android system is running. But sometime it reboot, and the boot type is watch dog.I 've kept record both of logcat and kmsg. But find nothing, it's so strange.!!

this is setting of watchdog:

<3>[ 14.988727] init: watchdogd:getsupport indent=0x8380
<3>[ 14.993958] init: watchdogd:getstatus flags=0x0
<3>[ 14.998648] init: watchdogd:getbootstatus flags=0x0
<3>[ 15.003757] init: watchdogd:gettimeout = 30
<3>[ 15.008113] init: watchdogd:getpretimeout = 5

if the reboot is caused by watchdog, why there is no exception or kernel crash or any other abnormal printing in kernel and logcat ? If not, what's this shit?

Labels (2)
0 Kudos
Reply
1 Reply

520 Views
Yuri
NXP Employee
NXP Employee

Hello,

 The watchdog usually provides SOC hardware reset, this does not allow using system interrupts.
Moreover, NXP recommends do not use just SOC reset, but - to implement total system POR instead,

via external circuit.

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 Kudos
Reply