Wakeup Source Configuration iMX8QXP/DX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Wakeup Source Configuration iMX8QXP/DX

7,103件の閲覧回数
jith
Contributor II

How to configure wakeup source in Cortex-m4 for iMX8QXP/DX.Planning to write mem to /sys/power/state entry and make the system into low power mode. Then need to wake up the system up using interface which is handled in Cortex-M4.

Could you please provide steps to configure wake source to preform the same.

ラベル(1)
0 件の賞賛
返信
6 返答(返信)

6,688件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jith

I am not aware of gpio wake examples, in general gpio wakeup

is implemented in the gpio-mxc driver, one can look at linux commits

MLK-19305-1 soc: imx: add PAD wakeup support
MLK-19305-2 gpio: mxc: add gpio PAD wakeup support
MLK-19305-3 arm64: enable gpio PAD wakeup for i.MX8 platforms   

linux-imx - i.MX Linux kernel 

linux-imx - i.MX Linux kernel 

linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

6,073件の閲覧回数
rob_mclean
Contributor IV

I found this topic helpful: "How to add iMX8QXP pad GPIO wakeup"

There is a presentation attached in that describes what changes to make to the device tree.

0 件の賞賛
返信

6,688件の閲覧回数
jith
Contributor II

Hi Igor,

Could you please share wake source example with w.r.to CortexM4.

By referring IMXLUG (Rev. L4.14.62_1.0.0_beta, 11/2018 ),I could configure the debug port as wake source as below and it works fine.

echo enabled > /sys/class/tty/ttymxc0/power/wakeup 

Some of the interfaces are handled from Cortex-M4 through RTOS.(Say flexcan).I would like to configure CAN as wake source and wake the system.

As part of my experiments I have done below

Step 1 : Configuring the wake source in CAN controller (RTOS configuration)

    • WAKSRC bit to 1
    • SLFWAK bit to 1

Step 2 : echo mem > /sys/power/state in Linux console and made  system to low power mode.

Step 3 : send CAN data to the system

Step 4 : checking wakeup is happened or not Linux - Not waking the system.

I could see in RM that iMXQ8XP interrupt logic are handled by IRQ STEER and GIC. 

IRQ-imx8QXp.PNG

I feel Cortex M4 interrupts are routed through IRQ steer logic and somewhere.Am I missing the wake source configuration something related same?

Could you please comment and  requesting to share if documentation is available on the same topic.

Thank you

0 件の賞賛
返信

6,688件の閲覧回数
vinothkumars
Senior Contributor IV

Hi jith‌,

Will you please give your configuration. I am also struggling in wake up.

 

 

Thanks & Regards,

VinothS,

Regards,
Vinothkumar Sekar
0 件の賞賛
返信

6,688件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jith

>I could see in RM that iMXQ8XP interrupt logic are handled by IRQ STEER and GIC

right, from software side it s handled by SCFW: SCFW Porting Kit

>Could you please share wake source example with w.r.to CortexM4.

>Could you please comment and  requesting to share if documentation is available on the same topic.

I am afraid such codes with w.r.to CortexM4 are not available yet, please note that

i.MX8QXP(DX) is preproduction processor and not officially supported. Also there is no

documentation on this subject. If you have project with such features suggest to

proceed with NXP Professional Services | NXP or apply to local NXP office for special support.

Best regards
igor

0 件の賞賛
返信

4,882件の閲覧回数
JesmithaMenezes
Contributor I

Hi, I am trying to enable flexcan as wakeup source at M4 core on iMX8DXL platform. May I know if this feature is supported on FreeRTOS. 

Also, could you please guide me on the same.

0 件の賞賛
返信