WM8960 driver porting in 3.14 kernel

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

WM8960 driver porting in 3.14 kernel

3,953件の閲覧回数
bandarulavanya
Contributor V

Hi all,

I am trying to use wm8960 in my kernel i can able to play what ever i recorded(arecord) using aplay But i am getting noise.

My MCLK is 24MHZ, SYSCLK-11.2896 and sample rate is 44.1. I am using LINPUT1 to Left out from Speaker i am using.

Kindly any one give the configurations for sample rates 16000, 8000, and 44100.

Thanks & Regards,

Lavanya

ラベル(2)
タグ(3)
0 件の賞賛
返信
3 返答(返信)

3,530件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Lavanya

please check patches on

https://community.nxp.com/docs/DOC-106295

https://community.nxp.com/thread/439583

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,531件の閲覧回数
bandarulavanya
Contributor V

Hi igorpadykov,

I tried those register settings but no use.

i am not able to get any thing. Is there any other settings, we are getting MCLK as 24MHz we probed with DSO.

Thanks

Lavanya

0 件の賞賛
返信

3,530件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Lavanya

typical bring-up procedure is to check codec clocks with oscilloscope,

use driver sources described in attached Linux Manual Table 28-1

Stereo Codec SoC Driver Files for debugging.

Best regards
igor

0 件の賞賛
返信