WLan Wandbaord DL IP Problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

WLan Wandbaord DL IP Problem

3,522 Views
Joerg-SH
Contributor III

Hello,

on my Wandboard DL I have running a Yocto Image I think it is the linaro Ubuntu roootfs.

My Problem is I want to use a static IP but when I do that WLan take the static IP and a DHCP IP.

wandboard192.168.2.2640:2C:F4:AE:1F:46 WLAN 13 Mbit/s
wandboard192.168.2.1140:2C:F4:AE:1F:46 WLAN 13 Mbit/s

someone could help on this?

regards  Joerg

Labels (3)
Tags (3)
0 Kudos
Reply
6 Replies

3,108 Views
OtavioSalvador
Senior Contributor II

I didn't get what you wish to do. Can you please elaborate?

For manual setting the WIFI you need wpa-supplication; for Yocto you'd most probably use connman and for Ubuntu you'd use NetworkManager. It has many possible ways of doing this so without a better understanding of your goal it is difficult to advice correctly.

0 Kudos
Reply

3,108 Views
Joerg-SH
Contributor III

I used the NetworkManager.

I conect the Board thru WLan to my WLan Router with static ip (192.168.2.11) but it is also conected by a second ip with same mac adress what i don´t want.

0 Kudos
Reply

3,108 Views
OtavioSalvador
Senior Contributor II

Can you paste the output of:

/sbin/ifconfig

/sbin/iwconfig

?

0 Kudos
Reply

3,108 Views
Joerg-SH
Contributor III

oot@wandboard:~# /sbin/ifconfig
eth2      Link encap:Ethernet  HWaddr 00:1f:7b:b2:05:f2 
          UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000
          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

lo        Link encap:Local Loopback 
          inet addr:127.0.0.1  Mask:255.0.0.0
          UP LOOPBACK RUNNING  MTU:16436  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:0
          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

wlan1     Link encap:Ethernet  HWaddr 40:2c:f4:ae:1f:46 
          inet addr:192.168.2.11  Bcast:192.168.2.255  Mask:255.255.255.0
          UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1
          RX packets:257 errors:0 dropped:51 overruns:0 frame:0
          TX packets:100 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000
          RX bytes:22238 (22.2 KB)  TX bytes:11560 (11.5 KB)

root@wandboard:~# /sbin/iwconfig
lo        no wireless extensions.

eth2      no wireless extensions.

wlan1     IEEE 802.11abg  ESSID:"FRITZ!Box Fon WLAN 7270" 
          Mode:Managed  Frequency:2.412 GHz  Access Point: BC:05:43:0F:65:33  
          Tx-Power=1496 dBm  
          Retry  long limit:7   RTS thr:off   Fragment thr:off
          Encryption key:off
          Power Management:on
          Link Quality=42/70  Signal level=-68 dBm 
          Rx invalid nwid:0  Rx invalid crypt:0  Rx invalid frag:0
          Tx excessive retries:0  Invalid misc:0   Missed beacon:0

0 Kudos
Reply

3,108 Views
OtavioSalvador
Senior Contributor II

Those seem right; so it seems you're calling the setup but not disabling Network Manager.

0 Kudos
Reply

3,108 Views
Joerg-SH
Contributor III

what could I do?  How to disabel Network Manager?

0 Kudos
Reply