WFI instruction

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

WFI instruction

跳至解决方案
2,114 次查看
takafuminaka
Contributor II

Hi chipexpert.


After returning from WFI instruction,  5% of our custom boards doesn't work properly.


For example, after calling WFI instruction,

PWM  doesn't output any signal(always LOW or HIGH) until 1msec timer interrupt happens.


Is there any procedure for using WFI instructnion?

Is it possible to use WFI instruction with iMX6 Solo processor?

Our BSP is "Custom Board" based Collage(by Sophia Systems Japan).


Regards,

Takafumi.

标签 (2)
标记 (1)
0 项奖励
回复
1 解答
1,914 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Takafumi

yes, definitely it is possible (and necessary)

to use WFI instruction with iMX6 Solo processor.

I would suggest to start search cause of this misbehaviour by narrowing

down possible reasons: software, hardware.

Please start with SDK low power test (SDK/apps/power_modes_test)

and check if it will work.

i.MX 6Series Platform SDK

Other option - run minimal image (without GPU,VPU, GUI).

This may point to power supply issues (spikes, bad filtering) on power lines.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,915 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Takafumi

yes, definitely it is possible (and necessary)

to use WFI instruction with iMX6 Solo processor.

I would suggest to start search cause of this misbehaviour by narrowing

down possible reasons: software, hardware.

Please start with SDK low power test (SDK/apps/power_modes_test)

and check if it will work.

i.MX 6Series Platform SDK

Other option - run minimal image (without GPU,VPU, GUI).

This may point to power supply issues (spikes, bad filtering) on power lines.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复