WARP7 can not output 3.3V

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

WARP7 can not output 3.3V

1,250 Views
chaunguyenngoc
Contributor III

I'm using a WARP7.

But when I check 3.3V with volmeter & led light.

I do not see any signal

- How can WARP7 output 3.3V ? (Software / hardware)

- is it broken ? (i'm just buy a new one)

Labels (1)
0 Kudos
Reply
2 Replies

1,175 Views
igorpadykov
NXP Employee
NXP Employee

Hi

please look at board schematic and identify how this voltage is produced

Design file for WaRP7 board (Schematics & P... | element14 | Technical Library 

then use sources for that board and try enable that output

Design file for WaRP7 board (Schematics & P... | element14 | Technical Library 

additional questions can be posted on dedicated to that board forum:

WaRP7 - The Next Generation IoT and Wearable De... | element14 | Design Center 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,175 Views
chaunguyenngoc
Contributor III

Hi igor

I read these file for times.

I think there is hardware problem.

You can check again if you have a warp7

About board forum, i will ask & check there too.

Thank you

0 Kudos
Reply