WARNING on building LF5.15.32_2.0.0 (Yocto 4.0 kirkstone)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

WARNING on building LF5.15.32_2.0.0 (Yocto 4.0 kirkstone)

2,007 Views
tanoue
Contributor III

I updated my BSP recipes from LF5.10.72_2.2.0(Yocto 3.3 hardknott) to LF5.15.32_2.0.0(Yocto 4.0 kirkstone)

 

My procedure was written in  "3 Host Setup" to "5 Image Build" of i.MX Yocto Project User's Guide.

 

After building, It seems the image file be built but the following WARNING was shown.

WARNING: imx-image-full-1.0-r0 do_rootfs: QA Issue: The license listed BSD was not in the licenses collected for recipe sigma-dut [license-file-missing]
WARNING: imx-image-full-1.0-r0 do_rootfs: QA Issue: The license listed BSD was not in the licenses collected for recipe sudo [license-file-missing]
WARNING: imx-image-full-1.0-r0 do_rootfs: QA Issue: The license listed BSD was not in the licenses collected for recipe sudo [license-file-missing]
WARNING: imx-image-full-1.0-r0 do_rootfs: QA Issue: The license listed BSD was not in the licenses collected for recipe sudo [license-file-missing]
WARNING: imx-image-full-1.0-r0 do_rootfs: QA Issue: The license listed BSD was not in the licenses collected for recipe wireless-tools [license-file-missing]

May I ignore these WARNINGs?

If not, how should these be resolved?

 

Best regards.

tanoue.

 

 

0 Kudos
Reply
6 Replies

1,995 Views
joanxie
NXP TechSupport
NXP TechSupport

what board do you use?

0 Kudos
Reply

1,992 Views
tanoue
Contributor III

Hi, @joanxie 

I used i.MX8M Plus EVK(8MPLUSLPD4-EVK).

 

Therefore, I entered the following command for setting build variables.

DISTRO=fsl-imx-xwayland MACHINE=imx8mp-lpddr4-evk source imx-setup-release.sh -b build-xwayland-kirkstone

Tags (1)
0 Kudos
Reply

1,988 Views
joanxie
NXP TechSupport
NXP TechSupport

you can ignore this warning

0 Kudos
Reply

1,985 Views
tanoue
Contributor III

Hi, @joanxie 

Why can I ignore this warning?

I will write image to my original board that designed referred EVK.

Even then, I'm wondering if it's okay to ignore it.

 

Best regards.

tanoue.

0 Kudos
Reply

1,980 Views
joanxie
NXP TechSupport
NXP TechSupport

do you have any issue with your built images? if no, you don't need care about this warning, I confirm this again for you

0 Kudos
Reply

1,974 Views
tanoue
Contributor III

I think my image's behavior is fine.

However, I worry about these WARNING may have some issue.

For example, if licenses of the recipes are not written in license.manifest in my yocto project.

If it occurs, I can't know all licenses in my product. This is a problem.

0 Kudos
Reply