Slow down access to quad SPI flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Slow down access to quad SPI flash

1,229 Views
BCVegas
Contributor I

I have a proto board with mismatched trace lengths between the processor and SPI flash memory, which is causing timing problems.  Is it possible to slow down the SPI interface in mcuxpresso to a speed to allow programming and access?

Labels (1)
0 Kudos
Reply
1 Reply

1,204 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Yes, customer can slow down the SPI Flash serial clock.

Just using SDK provided demo <flexspi_hyper_flash_polling_transfer>, the <app.h> has below function to initialise FlexSPI clock:

static inline void flexspi_clock_init(void)

Thanks for the attention.

Mike

0 Kudos
Reply