Vivante drivers for Xorg version 13

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Vivante drivers for Xorg version 13

1,537 Views
prathameshghane
Contributor II

Hello,

We are working on i.MX6 SABRE-AUTO board.

The board is currently using the uImage built from the BSP source L3.0.35_4.1.0_130816.

We are using Xorg driver:X.Org X Server 1.12.99.905 (1.13.0 RC 5).But, The VIVANTE .so files generated using LTIB are compatible with Xorg 10.0.

We get module version mismatch error when xorg tries to load vivante modules(.so's).

Hence, we seek help regarding Vivante drivers/libraries that are compatible with Xorg 13.0 and above.

Please let us know how we can get the above mentioned libs.

Thanks and regards,

Prathamesh Ghanekar

Labels (4)
0 Kudos
Reply
0 Replies