Vivante OpenGL headers location

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Vivante OpenGL headers location

跳至解决方案
3,801 次查看
matthewdavis
Contributor III

I'm looking for the headers for the OpenGL libraries that come in the fsl-proprietary bundle.  It looks like most of the time, you can simply use the mesa headers and the Vivante libraries, but there are extra functions that exist only in the vivante libraries, and I'm suspecting that some of the issues I'm running into may trace back to a mismatch between headers and libraries.  Are these headers distributed as part of any distribution?

标签 (3)
0 项奖励
回复
1 解答
3,557 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Matthew

one can look at sect.13.1.1.3 Source Code Structure

attached Linux Manual. Procedure of obtaining vivante gpu source code

is given in

About G2D API in i.MX6DQ.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,558 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Matthew

one can look at sect.13.1.1.3 Source Code Structure

attached Linux Manual. Procedure of obtaining vivante gpu source code

is given in

About G2D API in i.MX6DQ.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
3,557 次查看
matthewdavis
Contributor III

Thanks.  I've found exactly what I need now.

0 项奖励
回复