Virtual keyboard on Imx8 with weston

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Virtual keyboard on Imx8 with weston

2,074件の閲覧回数
arslan
Contributor III

In our project we are using Qt 5.15 with Wayland/Weston running on Imx8MPlus

Since now we could not magane to use any vistual keyboards (QtVirtualKeyboard, Maliit, Weston-keyboard..)

Everytime the reason from Qt side was, that weston and Qt are using different text input protocols. A workaround would be using another compositor instead of weston.

We need OpenGl acceleration which limits us here using another compositor,

for this see

https://community.nxp.com/t5/i-MX-Processors/Custom-wayland-compositor-on-IMX8M/td-p/976855

 

Anyone here who knows a solution with virtual keyboards, usable under Qt+Weston? What we cannot change is the CPU and Qt. 

 

ラベル(1)
0 件の賞賛
返信
0 返答(返信)