Video playback issues

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Video playback issues

1,511件の閲覧回数
IanCraig
Contributor II

Hi

I wonder if anyone can help with a couple of video playback issues.

My setup is a core-image-sato build with gstreamer and chromium using the "Fido" branch of the fsl-community-bsp and I am playing a H.264 video file.

1. Using the media player playback is good but if I put the display in to portrait mode using "xrandr" playback of the same video file is not good. CPU usage for gtk-play goes from 12% to 40%. Does anyone know if there are issues with hardware acceleration in portrait mode or a way to fix this.

2. I've built chromium but I can't play any H.264 files at all. Does anyone know if chromium can play these files or how I go about getting them to play.

Thanks

Ian

ラベル(5)
0 件の賞賛
返信
1 返信

1,376件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Ian,

Current xrand is supported however there are some features that are not accelerated by GPU, and this is marked as a bug.

Reduced graphic performance with rotated screen (imx6, sabresd)

Hope this helps

0 件の賞賛
返信