Video output on USB-C on imx8m plus

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Video output on USB-C on imx8m plus

ソリューションへジャンプ
6,371件の閲覧回数
inzenjer-banderas
Contributor I

Hello everybody,

We are planning to use an IMX8M PLUS based board for an embedded application which would include some sort of a screen to display graphical data. Since HDMI is not an option, I was wondering if it was possible to configure any Linux distribution/BSP to output video on its USB-C interface?

I must say that I am by no means expert in video related technologies and therefore couldn't find this information nor make much sense of other sources on the internet.

Best regards,

Lazar

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 解決策
6,362件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

The kernel 5.10 and up, can do that, but you will need to have a module that its not implemented for MX8MP.

Regards

 

元の投稿で解決策を見る

0 件の賞賛
返信
9 返答(返信)
6,353件の閲覧回数
inzenjer-banderas
Contributor I

Hello,

Thank you for your prompt answer. Just one more question, by module you mean software module, right?

Best Regards

0 件の賞賛
返信
6,000件の閲覧回数
guysoft
Contributor I

Hey,

Did you manage to figure out which driver/device tree setting is needed to get this to work?

Thanks!

0 件の賞賛
返信
6,344件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Yes, that's correct

0 件の賞賛
返信
6,338件の閲覧回数
inzenjer-banderas
Contributor I

Thank you very much.

Best regards

0 件の賞賛
返信
5,455件の閲覧回数
relaxibus
Contributor II
Hi, can you disclose if it works? I'm also looking for the same. Would like to use either VGA or HDMI.
0 件の賞賛
返信
5,445件の閲覧回数
inzenjer-banderas
Contributor I

Hello @relaxibus, at the end I  gave up trying to do it with USB, so I cannot confirm whether it works or not. Maybe somebody from NXP can tell us if that kernel module has been implemented for iMX8MP or not?

0 件の賞賛
返信
5,442件の閲覧回数
relaxibus
Contributor II
Thanks, I made a reply to NXP here, you can see the driver links now available for Ubuntu. May be it helps to achieve the goal.
0 件の賞賛
返信
6,363件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

The kernel 5.10 and up, can do that, but you will need to have a module that its not implemented for MX8MP.

Regards

 

0 件の賞賛
返信
5,443件の閲覧回数
relaxibus
Contributor II
Hi, I'm also looking for the same. Would like to use either VGA or HDMI. Will it works now with the USB 3.0 driver for Displaylink: https://www.synaptics.com/products/displaylink-graphics/downloads/ubuntu
https://support.displaylink.com/knowledgebase/articles/683482-displaylink-support-for-ubuntu-now-ava...
0 件の賞賛
返信