Video output on USB-C on imx8m plus

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Video output on USB-C on imx8m plus

跳至解决方案
5,788 次查看
inzenjer-banderas
Contributor I

Hello everybody,

We are planning to use an IMX8M PLUS based board for an embedded application which would include some sort of a screen to display graphical data. Since HDMI is not an option, I was wondering if it was possible to configure any Linux distribution/BSP to output video on its USB-C interface?

I must say that I am by no means expert in video related technologies and therefore couldn't find this information nor make much sense of other sources on the internet.

Best regards,

Lazar

标签 (2)
标记 (1)
0 项奖励
回复
1 解答
5,779 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

The kernel 5.10 and up, can do that, but you will need to have a module that its not implemented for MX8MP.

Regards

 

在原帖中查看解决方案

0 项奖励
回复
9 回复数
5,770 次查看
inzenjer-banderas
Contributor I

Hello,

Thank you for your prompt answer. Just one more question, by module you mean software module, right?

Best Regards

0 项奖励
回复
5,417 次查看
guysoft
Contributor I

Hey,

Did you manage to figure out which driver/device tree setting is needed to get this to work?

Thanks!

0 项奖励
回复
5,761 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Yes, that's correct

0 项奖励
回复
5,755 次查看
inzenjer-banderas
Contributor I

Thank you very much.

Best regards

0 项奖励
回复
4,872 次查看
relaxibus
Contributor II
Hi, can you disclose if it works? I'm also looking for the same. Would like to use either VGA or HDMI.
0 项奖励
回复
4,862 次查看
inzenjer-banderas
Contributor I

Hello @relaxibus, at the end I  gave up trying to do it with USB, so I cannot confirm whether it works or not. Maybe somebody from NXP can tell us if that kernel module has been implemented for iMX8MP or not?

0 项奖励
回复
4,859 次查看
relaxibus
Contributor II
Thanks, I made a reply to NXP here, you can see the driver links now available for Ubuntu. May be it helps to achieve the goal.
0 项奖励
回复
5,780 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

The kernel 5.10 and up, can do that, but you will need to have a module that its not implemented for MX8MP.

Regards

 

0 项奖励
回复
4,860 次查看
relaxibus
Contributor II
Hi, I'm also looking for the same. Would like to use either VGA or HDMI. Will it works now with the USB 3.0 driver for Displaylink: https://www.synaptics.com/products/displaylink-graphics/downloads/ubuntu
https://support.displaylink.com/knowledgebase/articles/683482-displaylink-support-for-ubuntu-now-ava...
0 项奖励
回复