Video output on USB-C on imx8m plus

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Video output on USB-C on imx8m plus

Jump to solution
5,811 Views
inzenjer-banderas
Contributor I

Hello everybody,

We are planning to use an IMX8M PLUS based board for an embedded application which would include some sort of a screen to display graphical data. Since HDMI is not an option, I was wondering if it was possible to configure any Linux distribution/BSP to output video on its USB-C interface?

I must say that I am by no means expert in video related technologies and therefore couldn't find this information nor make much sense of other sources on the internet.

Best regards,

Lazar

Labels (2)
Tags (1)
0 Kudos
Reply
1 Solution
5,802 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

The kernel 5.10 and up, can do that, but you will need to have a module that its not implemented for MX8MP.

Regards

 

View solution in original post

0 Kudos
Reply
9 Replies
5,793 Views
inzenjer-banderas
Contributor I

Hello,

Thank you for your prompt answer. Just one more question, by module you mean software module, right?

Best Regards

0 Kudos
Reply
5,440 Views
guysoft
Contributor I

Hey,

Did you manage to figure out which driver/device tree setting is needed to get this to work?

Thanks!

0 Kudos
Reply
5,784 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Yes, that's correct

0 Kudos
Reply
5,778 Views
inzenjer-banderas
Contributor I

Thank you very much.

Best regards

0 Kudos
Reply
4,895 Views
relaxibus
Contributor II
Hi, can you disclose if it works? I'm also looking for the same. Would like to use either VGA or HDMI.
0 Kudos
Reply
4,885 Views
inzenjer-banderas
Contributor I

Hello @relaxibus, at the end I  gave up trying to do it with USB, so I cannot confirm whether it works or not. Maybe somebody from NXP can tell us if that kernel module has been implemented for iMX8MP or not?

0 Kudos
Reply
4,882 Views
relaxibus
Contributor II
Thanks, I made a reply to NXP here, you can see the driver links now available for Ubuntu. May be it helps to achieve the goal.
0 Kudos
Reply
5,803 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

The kernel 5.10 and up, can do that, but you will need to have a module that its not implemented for MX8MP.

Regards

 

0 Kudos
Reply
4,883 Views
relaxibus
Contributor II
Hi, I'm also looking for the same. Would like to use either VGA or HDMI. Will it works now with the USB 3.0 driver for Displaylink: https://www.synaptics.com/products/displaylink-graphics/downloads/ubuntu
https://support.displaylink.com/knowledgebase/articles/683482-displaylink-support-for-ubuntu-now-ava...
0 Kudos
Reply