Video cropping on CSI->MEM path

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Video cropping on CSI->MEM path

ソリューションへジャンプ
2,047件の閲覧回数
henri_bragge
Contributor II

I have modified mxc_v4l2_tvin demo by adding VIDIOC_S_CROP call to crop the input frame. Cropping vertically (left/width) works just fine but when I crop horizontally (top/height), the image starts scrolling. The image seems to be cropped though, but I can't stabilize it.

Any ideas what could be wrong? On CSI->IC path cropping works OK.

I'm using MX537 CPU with Linux image based on 11.09.01 release (kernel 2.6.35.3).

ラベル(3)
タグ(3)
0 件の賞賛
返信
1 解決策
1,762件の閲覧回数
JayTu
NXP Employee
NXP Employee

My guessing is the hsync/vsync isn't match the size no matter vertically/horizontally scrolling.

You can try IPUx_CSIx_OUT_FRM_CTRL:CSIx_VSC (or related) increase/decrease value to suits your case.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,763件の閲覧回数
JayTu
NXP Employee
NXP Employee

My guessing is the hsync/vsync isn't match the size no matter vertically/horizontally scrolling.

You can try IPUx_CSIx_OUT_FRM_CTRL:CSIx_VSC (or related) increase/decrease value to suits your case.

0 件の賞賛
返信