Video Processing Latency

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Video Processing Latency

2,461 次查看
Pankh
Contributor I

Hello All,

System Overview:

Processor: iMX6 DualLite

Take the Video input from the camera, process the data and output it at ethernet or wifi.

Which camera interface (MIPI CSI2 or Parallel camera interface) of iMX6 I shall use to get the minimum latency in the output video data.

标签 (1)
0 项奖励
回复
2 回复数

2,230 次查看
SergioSolis
NXP Employee
NXP Employee

Hello Pankaj,

Saurabh is correct, a dual buffer approach is a good idea. If I had to make a recommendation, I would go with a MIPI camera.

0 项奖励
回复

2,230 次查看
saurabh206
Senior Contributor III

Hi

Pankaj

Latency is depends upon the how many buffers you have used with Camera interface.

Dual buffer approach provides latency of one frame.