Video Codecs issue on NXP im8 Quad max running Android Automotive 14

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Video Codecs issue on NXP im8 Quad max running Android Automotive 14

2,220件の閲覧回数
swayamdhondge10
Contributor II

I tried to run a video with mp4 extension on imx8 quad max board running android automotive 14 revision 17. For this, I have used the default available players like -

  1. Cactus Player - Unable to play the video.
  2. Gallery Video Player - Unable to play the video. 

Sharing the logs below. I have analysed the logs and I suspect there could be a codec issue. Additionally, I have installed and tested the VLC Player as it comes with the codecs and the video was playing. 

Previously, while working on Android Automotive 11 revision 40 on the same board (imx 8QM) -  video playback was working using the default players.

I am not sure whether the Android automotive 14 revision 17 built image is missing any video codec. Could someone please help understand / fix this issue. Any help would be greatly appreciated. 
Error logs : 
##########################
androidx.media3.exoplayer.ExoPlaybackException: MediaCodecVideoRenderer error, index=0, format=Format(1, null, null, video/mp4v-es, null, 19300153, null, [640, 510, 29.564842, ColorInfo(Unset color space, Unset color range, Unset color transfer, false, 8bit Luma, 8bit Chroma)], [-1, -1]), format_supported=YES
at androidx.media3.exoplayer.ExoPlayerImplInternal.handleMessage(ExoPlayerImplInternal.java:640)
at android.os.Handler.dispatchMessage(Handler.java:102)
at android.os.Looper.loopOnce(Looper.java:205)
at android.os.Looper.loop(Looper.java:294)
at android.os.HandlerThread.run(HandlerThread.java:67)
Caused by: androidx.media3.exoplayer.video.MediaCodecVideoDecoderException: Decoder failed: c2.imx.mpeg4.decoder
at androidx.media3.exoplayer.video.MediaCodecVideoRenderer.createDecoderException(MediaCodecVideoRenderer.java:1997)
at androidx.media3.exoplayer.mediacodec.MediaCodecRenderer.render(MediaCodecRenderer.java:893)
at androidx.media3.exoplayer.video.MediaCodecVideoRenderer.render(MediaCodecVideoRenderer.java:1033)
at androidx.media3.exoplayer.ExoPlayerImplInternal.doSomeWork(ExoPlayerImplInternal.java:1136)
at androidx.media3.exoplayer.ExoPlayerImplInternal.handleMessage(ExoPlayerImplInternal.java:561)
at android.os.Handler.dispatchMessage(Handler.java:102) 
at android.os.Looper.loopOnce(Looper.java:205) 
at android.os.Looper.loop(Looper.java:294) 
at android.os.HandlerThread.run(HandlerThread.java:67) 
Caused by: android.media.MediaCodec$CodecException: Error 0x16
2024-07-24 15:03:19.839 4384-5094 MediaCodec com.brouken.player E flush() is valid only at Executing states; currently at Released state
2024-07-24 15:03:19.840 4384-5052 ExoPlayerImplInternal com.brouken.player E Disable failed.
java.lang.IllegalStateException: flush() is valid only at Executing states; currently at Released state

at android.media.MediaCodec.native_flush(Native Method)
at android.media.MediaCodec.flush(MediaCodec.java:2504)
at androidx.media3.exoplayer.mediacodec.AsynchronousMediaCodecAdapter.flush(AsynchronousMediaCodecAdapter.java:247)
at androidx.media3.exoplayer.mediacodec.MediaCodecRenderer.flushCodec(MediaCodecRenderer.java:960)
at androidx.media3.exoplayer.mediacodec.MediaCodecRenderer.flushOrReleaseCodec(MediaCodecRenderer.java:953)
at androidx.media3.exoplayer.mediacodec.MediaCodecRenderer.onDisabled(MediaCodecRenderer.java:780)
at androidx.media3.exoplayer.video.MediaCodecVideoRenderer.onDisabled(MediaCodecVideoRenderer.java:809)
at androidx.media3.exoplayer.BaseRenderer.disable(BaseRenderer.java:220)
at androidx.media3.exoplayer.ExoPlayerImplInternal.disableRenderer(ExoPlayerImplInternal.java:1846)
at androidx.media3.exoplayer.ExoPlayerImplInternal.resetInternal(ExoPlayerImplInternal.java:1566)
at androidx.media3.exoplayer.ExoPlayerImplInternal.stopInternal(ExoPlayerImplInternal.java:1523)
at androidx.media3.exoplayer.ExoPlayerImplInternal.handleMessage(ExoPlayerImplInternal.java:686)
at android.os.Handler.dispatchMessage(Handler.java:102)
at android.os.Looper.loopOnce(Looper.java:205)
at android.os.Looper.loop(Looper.java:294)
at android.os.HandlerThread.run(HandlerThread.java:67)

 

 

 

0 件の賞賛
返信
0 返答(返信)