Value Change after Suspend to RAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Value Change after Suspend to RAM

1,521 Views
deepanrajanbara
Contributor IV

Hi,

Our is a custom board based on iMx6 and we are using Linux 3.10.53 kernel.The loops per jiffy value which is calibrated in kernel is getting change once the system resumes from suspend to ram, Because of which the delay which we have programmed in the driver gets changed and there is instability in the interface corresponding to the driver.What could be the reason for the change of loops per jiffy value after resuming from suspend to RAM.Please reply as soon as possible.

Thank you,

Deepanraj.A

0 Kudos
Reply
1 Reply

1,343 Views
igorpadykov
NXP Employee
NXP Employee

Hi Deepanraj

seems this is common linux problem as described on

https://www.kernel.org/doc/Documentation/timers/timekeeping.txt 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply