VPU use in xfreerdp

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VPU use in xfreerdp

1,128 Views
shlomz
Contributor III

Hi,

what plugin/s and changes are required for xfreerdp (2.8.1 or later) to use the VPU

on imx8mp for decoding incoming h.264 video frames?

 

thanks.

Tags (4)
0 Kudos
Reply
4 Replies

1,118 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Well, that depends on a lot of things:

  1. you need to have a session utilizing AVC444 mode (both, client and server! if only the client announces the format support it is not guaranteed that the server will use it)
  2. you need FFMPEG as h264 decoder as that one has some versions that utilize some hardware backed decoders (and you need to have one of these versions)

so, in case you have this FFMPEG the answer is: a little bit, otherwise no.
Why? RDP utilizes a non standard stream (2 H264 streams in YUV 4:2:2 mode recombined to one YUV4:4:4 image) so the decoded images must be copied back to system memory and the expensive operations are still done by the Core

so, if you have not enough Core you can ensure you utilize hardware accelerated SSL(that is actually the thing eating most Core with FreeRDP

 

You can check the note about share screen with freerdp:

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8DXL-screen-share-to-PC-by-using-Fre...

Regards

0 Kudos
Reply

1,114 Views
shlomz
Contributor III

I'm building the imx8mp image from yocto langdale (kernel 6.1) and I have ffmpeg installed (with libs)

Is there a specific way to build ffmpeg for that reason?

What switches other than AVC444 does xfreerdp requires? (gdi:hw ?)

I also updated free rdp to 3.x from the standard 2.8.1

0 Kudos
Reply

1,088 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

You can try the VPE plugin (used with ffmpeg) in following repositories from VeriSilicon, partner of NXP that provides Hantro VC8000D/VC8000E found in i.MX8MP : 

https://github.com/VeriSilicon/vpe

https://github.com/VeriSilicon/ffmpeg

It seems that they tested on iMX8MP.

Regards

0 Kudos
Reply

1,018 Views
shlomz
Contributor III

HI,

 

ffmpeg from the link is not being configured succesfully (pkg-config and other issues).

can you verify the fulle build?

 

thanks.

0 Kudos
Reply