VPU support format in i.MX6Dual

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

VPU support format in i.MX6Dual

1,353件の閲覧回数
keitanagashima
Senior Contributor I

Dear Sir or Madam,

Hello.

I have a question about VPU support format in i.MX6Dual.

[Q1]

Please tell me the input data format of H.264 Encoder.

(YUV NV12, YUV XXXX, RGB, etc)

[Q2]

Please tell me the output data format of H.264 Decoder.

(YUV NV12, YUV XXXX, RGB, etc)

Best Regards,

Keita

ラベル(6)
0 件の賞賛
返信
2 返答(返信)

1,042件の閲覧回数
Yuri
NXP Employee
NXP Employee

Please refer to section 69.6.3 (Video Codec Processing Buffer Requirement) of the i.MX6 SDL RM.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,042件の閲覧回数
keitanagashima
Senior Contributor I

Dear Yuri,

Hello.

Thank you for your reply.

I referred to section 69.6.3 (Video Codec Processing Buffer Requirement), but I didn't understand it.

What data format can VPU Encoder(H.264) input internally?

And, what format is it output when decoding H.264 in VPU decoder?

(Ex, YUV NV12, YUV XXXX, RGB, etc)

Best Regards,

Keita

0 件の賞賛
返信