VPU for WEC 2013

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

VPU for WEC 2013

1,408件の閲覧回数
rizwan_s
Contributor II

Hi,

I get the following error with VPU

\Wince800\iMX6Q_SABREAuto_ARMV7_Retail\cesysgen\platcomm\iMX6Q_SABREAuto\lib\ARMV7\retail\vpu_mx6q_fsl_v3.lib : fatal error LNK1136:invalid or corrupt file

"vpu_mx6q_fsl_v4.lib" is missing for WEC 2013.

Is there any way to get it in binary form?

I found the below thread

https://community.nxp.com/thread/323529

Is there any update available now for this issue?

Thanks and Regards

Rizwan Syed

ラベル(1)
0 件の賞賛
返信
1 返信

1,260件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Rizwan

nxp does not support wec for i.MX6, it may be suggested to

apply to third party support, as mentioned on that thread.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信