VPU for WEC 2013

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VPU for WEC 2013

1,409 Views
rizwan_s
Contributor II

Hi,

I get the following error with VPU

\Wince800\iMX6Q_SABREAuto_ARMV7_Retail\cesysgen\platcomm\iMX6Q_SABREAuto\lib\ARMV7\retail\vpu_mx6q_fsl_v3.lib : fatal error LNK1136:invalid or corrupt file

"vpu_mx6q_fsl_v4.lib" is missing for WEC 2013.

Is there any way to get it in binary form?

I found the below thread

https://community.nxp.com/thread/323529

Is there any update available now for this issue?

Thanks and Regards

Rizwan Syed

Labels (1)
0 Kudos
Reply
1 Reply

1,261 Views
igorpadykov
NXP Employee
NXP Employee

Hi Rizwan

nxp does not support wec for i.MX6, it may be suggested to

apply to third party support, as mentioned on that thread.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply