VPU firmware for i.MX6Solo.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

VPU firmware for i.MX6Solo.

ソリューションへジャンプ
2,972件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

I have some questions about i.MX6 VPU firmware.

In Linux BSP (L3.0.35_4.1.0), there are vpu firmwares in /lib/firmware.

Then, please see my questions below.

[Q1]

I want to know whether I can use vpu_fw_imx6q.bin for i.MX6Solo.

I think I can use it because i.MX6Solo has same VPU as i.MX6 Quad.

Is this correct?

Or there is a binary for i.MX6Solo?

[Q2]

If the answer for Q1 is "correct", i.MX6SDL and i.MX6DQ can use same binary file, isn't it?

However, there is vpu_fw_imx6d.bin in same directory.

What is this?

There is no description about this binary in i.MX_6Dual6Quad_VPU_API_Reference_Manual.pdf in Linux BSP documentation.

Best Regards,

Satoshi Shimoda

ラベル(6)
タグ(1)
0 件の賞賛
返信
1 解決策
2,307件の閲覧回数
max_tsai
NXP Employee
NXP Employee

hi,

vpu_fw_imx6q.bin is for i.MX6DQ

vpu_fw_imx6d.bin is for i.MX6DL & i.MX6Solo.

Regards,

Max

元の投稿で解決策を見る

0 件の賞賛
返信
8 返答(返信)
2,307件の閲覧回数
max_tsai
NXP Employee
NXP Employee

hi,

Checked with VPU owner. i.MX6Solo use "vpu_fw_imx6d.bin".

The two binraries are for i.MX6DQ and i.MX6DL respectively.

Regards,

Max

0 件の賞賛
返信
2,307件の閲覧回数
satoshishimoda
Senior Contributor I

Hi Mix Tsai,

> Checked with VPU owner. i.MX6Solo use "vpu_fw_imx6d.bin".

> The two binraries are for i.MX6DQ and i.MX6DL respectively.

Excuse me, what is " The two binraries"?

According to your reply, I understood as following, is this correct?

i.MX6DL & i.MX6DQ => vpu_fw_imx6q.bin

i.MX6S => vpu_fw_imx6d.bin

Best Regards,

Satoshi Shimoda

0 件の賞賛
返信
2,308件の閲覧回数
max_tsai
NXP Employee
NXP Employee

hi,

vpu_fw_imx6q.bin is for i.MX6DQ

vpu_fw_imx6d.bin is for i.MX6DL & i.MX6Solo.

Regards,

Max

0 件の賞賛
返信
2,307件の閲覧回数
satoshishimoda
Senior Contributor I

Can anybody reply me?

0 件の賞賛
返信
2,307件の閲覧回数
YixingKong
Senior Contributor IV

Satoshi

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 件の賞賛
返信
2,307件の閲覧回数
satoshishimoda
Senior Contributor I

Hi Yixing Kong,

Sorry for delay.

I have not understood well about Q1 and Q2 yet.

So I would appreciate it if you answer my questions.

Best Regards,

Satoshi Shimoda

0 件の賞賛
返信
2,307件の閲覧回数
YixingKong
Senior Contributor IV

Satoshi-san

I will see if I can assign your questions to our AE.

Thanks,

Yixing

0 件の賞賛
返信
2,307件の閲覧回数
YixingKong
Senior Contributor IV

Satoshi

We are sorry for getting back to you so late. Are you still stuck with the issue? If you have somehow resolved the issue, can we close the discussion? If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 件の賞賛
返信