VPU errors when dual-direction video streaming

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VPU errors when dual-direction video streaming

4,135 Views
ripple
Contributor I

I met a dual-direction video streaming question when using camera for video phone application, seems some troubles come from VPU.

I had two i.mx53 board with camera, one's ip is 192.168.0.202, the other's is 192.168.0.210. Used following command line as video streaming receiver:

gst-launch-0.10 -v udpsrc port=5002 ! queue ! capsfilter caps="application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H264, profile-level-id=(string)420014, payload=(int)96" ! rtph264depay ! mfw_vpudecoder codec-type=std_avc ! queue ! mfw_isink sync=false async=false

Used following command line as video streaming transmitter:

gst-launch-0.10 -v mfw_v4lsrc capture-width=352 capture-height=288 ! queue ! mfw_vpuencoder codec-type=std_avc ! rtph264pay ! queue ! udpsink host=192.168.0.202 port=5002 sync=false async=false

All single direction video communication worked well, but if I used dual direction command line like a video phone, the error came out .

I ran this command line on 192.168.0.102

gst-launch-0.10 -v udpsrc port=5002 ! queue ! capsfilter caps="application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H264, profile-level-id=(string)420014, payload=(int)96" ! rtph264depay ! mfw_vpudecoder codec-type=std_avc ! queue ! mfw_isink sync=false async=false &

gst-launch-0.10 -v mfw_v4lsrc capture-width=352 capture-height=288 ! queue ! mfw_vpuencoder codec-type=std_avc ! rtph264pay ! queue ! udpsink host=192.168.0.210 port=5010 sync=false async=false

And ran  this command line on 192.168.0.102

gst-launch-0.10 -v udpsrc port=5010 ! queue ! capsfilter caps="application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H264, profile-level-id=(string)420014, payload=(int)96" ! rtph264depay ! mfw_vpudecoder codec-type=std_avc ! queue ! mfw_isink sync=false async=false &

gst-launch-0.10 -v mfw_v4lsrc capture-width=352 capture-height=288 ! queue ! mfw_vpuencoder codec-type=std_avc ! rtph264pay ! queue ! udpsink host=192.168.0.202 port=5002 sync=false async=false

Both mx53 boards came out such log line text every second:

"[WARN] VPU mutex couldn't be locked before timeout expired"

And the screen freezed and no any video playing.

Can anybody give me some suggestion? Thank you!

Tags (1)
0 Kudos
Reply
4 Replies

3,620 Views
ripple
Contributor I

Yeah! 

The "loopback" parameter worked well in MPEG-4 format streaming. 

Still have problem in H.264 streaming. I will trace it in detail.

Lots of thank to Daiane ! :-)

0 Kudos
Reply

3,620 Views
daiane_angolini
NXP Employee
NXP Employee

yes, try it with true (loopback=true)

it will allow gst plugin to create thread properly to configure VPU to have 2 simultaneous instances (one for decoder and one for encoder just like a loopback)

0 Kudos
Reply

3,620 Views
ripple
Contributor I

yes, it has, default value is false. 

Is it needed to be true? Can you tell me what this property's function is? Some confused by the inspect log line.

Thank you, Daiane!

0 Kudos
Reply

3,620 Views
daiane_angolini
NXP Employee
NXP Employee

Can you, please, see if your vpuencoder / vpudecoder has a loopback property?

gst-inspect mfw_vpudecoder | grep loopback

0 Kudos
Reply