VPU encoding I frame problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

VPU encoding I frame problem

1,489件の閲覧回数
juzichen
Contributor I

Hi,All

Before I start coding will gopSize value is set to 10, but only at the beginning of the video I frame, the rest all the P frame, what reason is this excuse me?

wxid_j12r32y9s5p322_1481254146535_79.png

 

L3.0.35

 

Hope for your help!

Regards.

0 件の賞賛
返信
1 返信

1,403件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

there are lots of similar requests based on different application or customer, So our vpu encoder just only provide the basic operation, and it is user's responsibility to implement complex combination.
In fact, the two requirements(IDR and SPS/PPS header) was implemented in our framework but not vpu encoder.

customre should rewrite the software by themselves

0 件の賞賛
返信