VPU Error during WFD

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

VPU Error during WFD

1,510 次查看
saurabh206
Senior Contributor III

Hi,

I am using Android 4.3 for IMX6Q based custom hardware.

I am getting following error while trying to start WFD.

What is a significance of following VPU error?

I/vpu-lib ( 2359): <gpu> alloc handle: 0x41781278, paddr: 0x7365b000, vaddr: 0x472a0000

I/vpu-lib ( 2359): <gpu> alloc handle: 0x41592548, paddr: 0x7632c000, vaddr: 0x49f71000

I/vpu-lib ( 2359): <gpu> alloc handle: 0x41592590, paddr: 0x78c30000, vaddr: 0x4c875000

I/vpu-lib ( 2359): <gpu> alloc handle: 0x41760fc8, paddr: 0x78d83000, vaddr: 0x4c9c8000

I/OMXPlayer( 2359): LEVEL: 1 FUNCTION: VPUCom_Init LINE: 236

I/OMXPlayer( 2359): VPUCom_Init: vpu open failure: ret=0x1

I/OMXPlayer( 2359): LEVEL: 1 FUNCTION: FilterOneBuffer LINE: 2372

I/OMXPlayer( 2359): FilterOneBuffer: vpu init failure: ret=0x1

E/ACodec  ( 2359): [OMX.Freescale.std.video_encoder.avc.hw-based] ERROR(0x8000100b)

E/MediaCodec( 2359): Codec reported an error. (omx error 0x8000100b, internalError -2147483648)

Regards,

Saurabh

标记 (3)
0 项奖励
回复
2 回复数

1,188 次查看
saurabh206
Senior Contributor III

Hi,

Bio

Thanks for the reply.

I am using Android 4.3 provided by Freescale only.

I will follow suggested document.

Regards

Saurabh

0 项奖励
回复

1,188 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

You are using the omx player kk version instead of wfdsink please review the "i.MX Android Extended Codec Release Notes" document in order to apply specific patches to add more multimedia format support on i.MX based board.

Regards

0 项奖励
回复