VPU Error during WFD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VPU Error during WFD

1,504 Views
saurabh206
Senior Contributor III

Hi,

I am using Android 4.3 for IMX6Q based custom hardware.

I am getting following error while trying to start WFD.

What is a significance of following VPU error?

I/vpu-lib ( 2359): <gpu> alloc handle: 0x41781278, paddr: 0x7365b000, vaddr: 0x472a0000

I/vpu-lib ( 2359): <gpu> alloc handle: 0x41592548, paddr: 0x7632c000, vaddr: 0x49f71000

I/vpu-lib ( 2359): <gpu> alloc handle: 0x41592590, paddr: 0x78c30000, vaddr: 0x4c875000

I/vpu-lib ( 2359): <gpu> alloc handle: 0x41760fc8, paddr: 0x78d83000, vaddr: 0x4c9c8000

I/OMXPlayer( 2359): LEVEL: 1 FUNCTION: VPUCom_Init LINE: 236

I/OMXPlayer( 2359): VPUCom_Init: vpu open failure: ret=0x1

I/OMXPlayer( 2359): LEVEL: 1 FUNCTION: FilterOneBuffer LINE: 2372

I/OMXPlayer( 2359): FilterOneBuffer: vpu init failure: ret=0x1

E/ACodec  ( 2359): [OMX.Freescale.std.video_encoder.avc.hw-based] ERROR(0x8000100b)

E/MediaCodec( 2359): Codec reported an error. (omx error 0x8000100b, internalError -2147483648)

Regards,

Saurabh

Tags (3)
0 Kudos
Reply
2 Replies

1,182 Views
saurabh206
Senior Contributor III

Hi,

Bio

Thanks for the reply.

I am using Android 4.3 provided by Freescale only.

I will follow suggested document.

Regards

Saurabh

0 Kudos
Reply

1,182 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

You are using the omx player kk version instead of wfdsink please review the "i.MX Android Extended Codec Release Notes" document in order to apply specific patches to add more multimedia format support on i.MX based board.

Regards

0 Kudos
Reply