VGA monitor is not displaying anything after connecting to IMX6Q board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VGA monitor is not displaying anything after connecting to IMX6Q board

1,208 Views
virendrasingh
Contributor I

Hi All,

     I have received new iMX6q board and have done following steps for bring it up:-

     1. Inserted SD card

     2. Connected USB Debug cable.

     3. Connected HDMI Cable (used HDMI to VGA converter to connect the board with VGA monitor)

     4. Connected lan cable to ethernet port.

     5. Connected power supply.

     After completion of booting the board, VGA monitor is not displaying anything. I am getting below log messages in teraterm:-

       mxc_hdmi mxc_hdmi: Read EDID again

mxc_hdmi mxc_hdmi: No modes read from edid

mxc_hdmi mxc_hdmi: create default modelist

fbcvt: 1920x1080@60: CVT Name - 2.073M9.

Please, provide us your valuable suggestion.

Thanks.

Labels (1)
0 Kudos
Reply
1 Reply

1,056 Views
Yuri
NXP Employee
NXP Employee

HDMI I/F should not be used with HDMI-to-DVI converter.
Please try using "true" HDMI monitor / TV.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply