VDDARM Voltage

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VDDARM Voltage

3,144 Views
darrellblock
NXP Employee
NXP Employee

What is the Freescale recommended operation mode for the VDDARM voltage if the design uses the MMPF0100 PMIC?  Our Design implementation for the PMIC matches the Sabre Smart Devices Platform.  

Is there any advantage to running in the Analog regulation mode if PMIC supplies the ARM and the SOC voltage from separate buck converters as the PMIC MMPF0100?

If you are using the Analog regulation mode, why bother to change voltage when the CPU changes frequency since a voltage change will just dissipate the power in the internal LDO which is in the iMX6?  

.

Labels (1)
2 Replies

2,558 Views
AnsonHuang
NXP Employee
NXP Employee

Hi, Darrell

     If you have an external PMIC,  to save power, we should use LDO bypass mode, which means internal analog regulator is bypassed, this is also our default setting of BSP.

0 Kudos
Reply

2,558 Views
Yuri
NXP Employee
NXP Employee

  IMX6 Datasheet(s) [say, Table 6 (Operating Ranges) of IMX6DQCEC, rev. 2.3, 07_2013] provide

VDDARM_IN (VDDSOC_IN) power supply specs for two options : LDO enabled and LDO bypassed.

The first case is used for cases when internal regulars are applied to supply internal i.MX6 modules;

the second one is intended for external supply only . The first case is recommended because

internal regulators are tested and proven for processor operations, DVFS approach in (Linux) BSP
uses this case. As for additional consumption, concerned with the regulators – this is optimized and

not very critical.  

0 Kudos
Reply