Using tja1463 instead of tjr1443

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using tja1463 instead of tjr1443

789 次查看
DusanStanisic99
Contributor II

Hello everyone,

We are working on enabling TJA1463 CAN transceivers on a custom board.

While reviewing the can-phy-transceiver.c file in <kernel>/drivers/phy/ inside linux-imxversion 6.6 (link), we observed that it is compatible with the TJR1443 CAN transceiver. Additionally, the TJA1463 appears to be backward compatible with previous versions of the TJx14 series.

tja1463.png

Assuming no major differences between these two transceivers (apart from the maximum bitrate), can we simply add a new section to the compatibility field and update the device tree source (DTS) files where necessary, and expect it to function correctly?

snippet.png

 

0 项奖励
回复
1 回复

748 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

If no more modification need in the dtb is suppose to work.

Regards

0 项奖励
回复