Using third party Libraries

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using third party Libraries

1,437 Views
chandraevolute
Contributor V


Hi ,

I am using third part source files, cross compiling them and generating the shared library.

I am using imx6ulevk, poky version 1.8. I am able to generate the shared libraries.

And i wrote a sample application using the shared library and crosscompiled and generated the executable.

When I am trying to run the executable say

./Example it is giving a error like libMso.so cannot be opened . File is missing.

I copied the libraries to /usr/lib/ still the error comes.

Do i need to build the RFS again by copying these libraries ??

Labels (3)
0 Kudos
Reply
1 Reply

1,375 Views
igorpadykov
NXP Employee
NXP Employee

Hi chandra

libraries may be compiled with different toolchain, so

indeed there may be necessary to build the RFS again.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply