Using the i.MX53 UART CTS signal for automatic transmission control.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Using the i.MX53 UART CTS signal for automatic transmission control.

跳至解决方案
1,426 次查看
mmichaelis
Contributor I
Can the UART on the i.MX53 use the CTS signal to automatically enable when transmitting and disable at the end of transmission.This would be useful for doing half-duplex RS-485 communications.
标签 (1)
标记 (2)
0 项奖励
回复
1 解答
1,225 次查看
igorpadykov
NXP Employee
NXP Employee

Hi mmichaelis

unfortunatey not, i.MX53 UART does not fully support RS485 mode

(in particular direction control), opposite to i.MX6 UART, which supports that.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,226 次查看
igorpadykov
NXP Employee
NXP Employee

Hi mmichaelis

unfortunatey not, i.MX53 UART does not fully support RS485 mode

(in particular direction control), opposite to i.MX6 UART, which supports that.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复