Using the QuadSPI Flash on i.MX7 SABRE SDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using the QuadSPI Flash on i.MX7 SABRE SDB

1,609 Views
daweichen
Contributor III

The NXP i.MX7 SABRE SDB has a on QSPI flash memory.  The schematic shows a MX25L51245GZ2I-10G device is populated. The schematic also indicates moving/removing some resistors.

In addition to the resistor changes and SW2 Boot Config setting, are there instructions for programming and erasing the on-board QuadSPI flash memory device?

At minimum, I would like to download a U-Boot image to the flash memory, so I can at least boot the SABRE SDB and load a Linux OS over a Ethernet network.

Thank you very much,

Dawei

Labels (2)
0 Kudos
Reply
1 Reply

847 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dawei

for programming qspi please use MFG Tool and script
mfgtool2-yocto-mx-sabresd-qspi-nor-mx25l51245g.vbs, check documentation inside package

Programmers (Flash, etc.) (2)
IMX6_L4.1.15_1.2.0_MFG_TOOL (REV L4.1.15_1.2.0)

One can use Demo Files:

Recommended Software & Tools (5)
 L4.1.15_1.2.0_iMX7D (REV L4.1.15_1.2.0)
i.MX 7Dual SABRESD Linux Binary Demo Files
http://www.nxp.com/products/software-and-tools/hardware-development-tools/sabre-development-system/s...


Recommended reading (pay attention to i.MX_Linux_User's_Guide.pdf included in L4.1.15_1.2.0_LINUX_DOCS):

Users Guides (1)
SABRE SDB for i.MX 7Dual - Quick Start Guide
Supporting Information (4)
L4.1.15_1.2.0_LINUX_DOCS
http://www.nxp.com/products/software-and-tools/hardware-development-tools/sabre-development-system/s...
Getting Started
http://www.nxp.com/products/software-and-tools/hardware-development-tools/sabre-development-system/s...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply