Using rpm -i on b4860qds

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using rpm -i on b4860qds

1,136 次查看
chandramills
Contributor I

I build several gnu packages using the yocto environment.  I copy the packages onto a USB stick and put the stick into the b4860.  It mounts and I try to install the packages but notfhing happens.  Can anyone help?

C_

root@b4860qds:/run/media/sda1/ppc64# rpm -i gnuradio-3.7.5-r0.ppc64e6500.rpm

root@b4860qds:/run/media/sda1/ppc64#

root@b4860qds:/run/media/sda1/ppc64# which rpm

/bin/rpm

root@b4860qds:/run/media/sda1/ppc64# rpm --help

BusyBox v1.23.2 (2016-05-15 09:55:50 CST) multi-call binary.

Usage: rpm -i PACKAGE.rpm; rpm -qp[ildc] PACKAGE.rpm

root@b4860qds:/run/media/sda1/ppc64#

0 项奖励
回复
1 回复

1,056 次查看
Pavel
NXP Employee
NXP Employee

See FAQ for SDK:

https://freescale.sdlproducts.com/LiveContent/web/pub.xql?action=home&pub=QorIQ_LS2085A_EAR_6.0&lang...

This FAQ recommends adding new package to he host PC before image building.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复