Using qt in I.MX6UL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Using qt in I.MX6UL

跳至解决方案
2,917 次查看
JHY
Contributor IV

I.MX6UL has no accelerator for 2D/3D.

Does it mean that I.MX6UL can't use QT applications at all?

标签 (1)
标记 (1)
1 解答
2,465 次查看
igorpadykov
NXP Employee
NXP Employee

Hi JHY

in general it can use as discussed on meta-fsl-arm mailing list:

Freescale OpenEmbedded/Yocto Layers discussion list ()

however it is not supported in official bsp, refer to attached Release Notes p.8.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
2,466 次查看
igorpadykov
NXP Employee
NXP Employee

Hi JHY

in general it can use as discussed on meta-fsl-arm mailing list:

Freescale OpenEmbedded/Yocto Layers discussion list ()

however it is not supported in official bsp, refer to attached Release Notes p.8.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------