Using imx53 pmic 34708 question ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using imx53 pmic 34708 question ?

2,652 Views
BruceYang
Contributor I

Hello, everybody, I have some questions I would like to ask a new pmic mc34708 freescale imx53 board to test results after I compile the overall completion failure usb host, and touch not encountered problems people do not know it? Thank!!

Labels (2)
Tags (1)
0 Kudos
Reply
3 Replies

2,082 Views
Yongxin
NXP Employee
NXP Employee

Are you using Freescale i.MX53-START-R(MC34708+i.MX535) or the board is designed by yourself?

If you designed the board, please attached your schematic

0 Kudos
Reply

2,082 Views
BruceYang
Contributor I

i using L2.6.35_11.09.01_ER_docs.tar.gz  & patches.tar.gz form Official Website.

Use these packaging to compile, compile results for success, but the touch as well as USB will not work

da9052_ssc_i2c 0-0048: 2 - da9052_i2c_read:master_xfer Failed!!

da9052_i2c_is_connected - i2c read failed.....

da9052_ssc_i2c 0-0048: 2 - da9052_i2c_read:master_xfer Failed!!

da9052_i2c_is_connected - i2c read failed.....

No device for codec mxc spdif

No device for DAI mxc spdif

No device for DAI imx-ssi-1-0

No device for DAI imx-ssi-1-1

No device for DAI imx-ssi-2-0

No device for DAI imx-ssi-2-1

No device for DAI imx-spdif-dai

cp: writing `/mnt/rwfs/var/lib/rpm/Basenames': No space left on device

cp: writing `/mnt/rwfs/var/lib/rpm/Group': No space left on device

cp: writing `/mnt/rwfs/var/lib/rpm/Conflictname': No space left on device

cp: writing `/mnt/rwfs/var/lib/rpm/Filemd5s': No space left on device

cp: writing `/mnt/rwfs/var/lib/rpm/Name': No space left on device

cp: writing `/mnt/rwfs/var/lib/rpm/Sigmd5': No space left on device

cp: writing `/mnt/rwfs/var/lib/rpm/Sha1header': No space left on device

cp: writing `/mnt/rwfs/var/lib/rpm/Triggername': No space left on device

cp: writing `/mnt/rwfs/var/lib/rpm/Packages': No space left on device

cp: writing `/mnt/rwfs/var/lib/rpm/Requireversion': No space left on device

cp: writing `/mnt/rwfs/var/lib/rpm/Requirename': No space left on device

cp: writing `/mnt/rwfs/var/lib/rpm/Provideversion': No space left on device

cp: writing `/mnt/rwfs/var/lib/rpm/Dirnames': No space left on device

cp: writing `/mnt/rwfs/var/state/dhcp/dhclient.leases': No space left on device

cp: writing `/mnt/rwfs/var/state/dhcp/dhcpd.leases': No space left on device

mount: mounting usbfs on /proc/bus/usb failed: No such file or directory

0 Kudos
Reply

2,082 Views
Yongxin
NXP Employee
NXP Employee

1. touch: please select MC34708 ADC driver in Linux Kernel.

2. please check if Vbus power is applied.

0 Kudos
Reply