Using imx27 VPU lib?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using imx27 VPU lib?

ソリューションへジャンプ
5,344件の閲覧回数
zhangjay
Contributor II

Is there any source code about imx27(or other freescale CPU) VPU application, I just want to encode the camera data to H264?

Anyone can provide me some sample code?

Thanks anyway!

0 件の賞賛
返信
1 解決策
5,194件の閲覧回数
liangyu
Contributor III

Yes,you can download mediacodec from freescale

元の投稿で解決策を見る

0 件の賞賛
返信
8 返答(返信)
5,194件の閲覧回数
liangyu
Contributor III

you can get it from Linux source files. It include freescale's plugins of gstreamer!

0 件の賞賛
返信
5,194件の閲覧回数
JayZhang
Fresh Out Contributor

Are you come from China?

I guess you are from China, because of your name~~

0 件の賞賛
返信
5,195件の閲覧回数
liangyu
Contributor III

Yes,you can download mediacodec from freescale

0 件の賞賛
返信
5,194件の閲覧回数
JayZhang
Fresh Out Contributor

我是江苏的,msn:[email protected]

qq:417248058,加个好友吧~~呵呵

0 件の賞賛
返信
5,194件の閲覧回数
liangyu
Contributor III

maybe you can read the gstreamer plugins about encode!

0 件の賞賛
返信
5,194件の閲覧回数
JayZhang
Fresh Out Contributor

Where I can download the gstream source?

0 件の賞賛
返信
5,194件の閲覧回数
zhangjay
Contributor II

Anyone can help me?

0 件の賞賛
返信
5,195件の閲覧回数
JayZhang
Fresh Out Contributor

The same question!

0 件の賞賛
返信