Using imx27 VPU lib?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using imx27 VPU lib?

Jump to solution
5,258 Views
zhangjay
Contributor II

Is there any source code about imx27(or other freescale CPU) VPU application, I just want to encode the camera data to H264?

Anyone can provide me some sample code?

Thanks anyway!

0 Kudos
Reply
1 Solution
5,108 Views
liangyu
Contributor III

Yes,you can download mediacodec from freescale

View solution in original post

0 Kudos
Reply
8 Replies
5,108 Views
liangyu
Contributor III

you can get it from Linux source files. It include freescale's plugins of gstreamer!

0 Kudos
Reply
5,108 Views
JayZhang
Contributor I

Are you come from China?

I guess you are from China, because of your name~~

0 Kudos
Reply
5,109 Views
liangyu
Contributor III

Yes,you can download mediacodec from freescale

0 Kudos
Reply
5,108 Views
JayZhang
Contributor I

我是江苏的,msn:[email protected]

qq:417248058,加个好友吧~~呵呵

0 Kudos
Reply
5,108 Views
liangyu
Contributor III

maybe you can read the gstreamer plugins about encode!

0 Kudos
Reply
5,108 Views
JayZhang
Contributor I

Where I can download the gstream source?

0 Kudos
Reply
5,108 Views
zhangjay
Contributor II

Anyone can help me?

0 Kudos
Reply
5,109 Views
JayZhang
Contributor I

The same question!

0 Kudos
Reply